Post Go back to editing

Hardware Setup on ADZS-AD2428MINI, EVAL-ADUSB2Z and molex ROAD NOISE CANCELLATION (RNC SENSOR SYSTEM)

Category: Hardware
Product Number: ADZS-AD2428MINI, EVAL-ADUSB2Z and molex ROAD NOISE CANCELLATION (RNC SENSOR SYSTEM)
Software Version: SigmaStudio Version 4.7

hi everyone,

i'm new to learn about the analog devices and to do my project i need help.

i have a  ADZS-AD2428MINI board and a  EVAL-ADUSB2Z  from ANALOG DEVICES and by using these boards i want to program a  ROAD NOISE CANCELLATION (RNC) SENSOR. i started to read "A2B Quick Start Guide" and installed sigmaStudio.

i don't know how to setup the hardware because my board is different to the boards wrote in the tutorial. could you please help me and tell me what can i do. thanks in advanced

Parents
  • Hi ladan,

    Thanks for contacting A2B support.

    ADZS-AD2428MINI board is a break-out board which can interface with EV-SOMCRR-EZKIT (via a 100-pin connector) or any custom board (via a 32 pin 0.1" header). You'd need a board which has Sigma DSP like ADAU1452/ADAU1451 as the A2B Main node etc. to program the board using Sigma Studio and EVAL-ADUSB2Z.

    Could you please confirm if you already have EV-SOMCRR-EZKIT?

    A supported SOM board needs to be attached to EV-SOMCRR-EZKIT along with ADZS-AD2428MINI which can act as A2B Main node. The example projects for this setup can be found in "C:\Analog Devices\ADI_A2B_Software-Rel19.x.x\Target\examples" folder. 

    If not, you can use EVAL-AD2428WD1BZ board as A2B Main node which can be directly programmed using Sigma Studio.

    Thanks

    Shibin

Reply
  • Hi ladan,

    Thanks for contacting A2B support.

    ADZS-AD2428MINI board is a break-out board which can interface with EV-SOMCRR-EZKIT (via a 100-pin connector) or any custom board (via a 32 pin 0.1" header). You'd need a board which has Sigma DSP like ADAU1452/ADAU1451 as the A2B Main node etc. to program the board using Sigma Studio and EVAL-ADUSB2Z.

    Could you please confirm if you already have EV-SOMCRR-EZKIT?

    A supported SOM board needs to be attached to EV-SOMCRR-EZKIT along with ADZS-AD2428MINI which can act as A2B Main node. The example projects for this setup can be found in "C:\Analog Devices\ADI_A2B_Software-Rel19.x.x\Target\examples" folder. 

    If not, you can use EVAL-AD2428WD1BZ board as A2B Main node which can be directly programmed using Sigma Studio.

    Thanks

    Shibin

Children