Post Go back to editing

How to configure ADZS-AD2428MINI with Sigma Studio?

Category: Software
Software Version: Version 4.6. Build 0, Rev. 1812

I am a new user of Sigma Studio and A2B devices.
I have the ADZS-AD2428MINI as a master and EVAL-AD2428WG1BZ as a slave device.
My idea was to create schematics for my devices but I could not manage to add ADZS-AD2428MINI to my schematics sheet.
So, the question is how to add it, or is there any alternative for this ADZS-AD2428MINI device?

Parents
  • Hi vuleta,

       if it can be useful, I'm working without problems on my custom setup made up of

    - n. 2  ADZS-AD2428MINI as A2B Master and Slave nodes (just drive I2C pins on the Master node board using USBi)

    - n. 2 EVAL-ADAU1467Z as Audio Host and Audio Sink (programmed via SPI by two STM32 microcontrollers in my case, but you can program them directly using Sigma Studio)

Reply
  • Hi vuleta,

       if it can be useful, I'm working without problems on my custom setup made up of

    - n. 2  ADZS-AD2428MINI as A2B Master and Slave nodes (just drive I2C pins on the Master node board using USBi)

    - n. 2 EVAL-ADAU1467Z as Audio Host and Audio Sink (programmed via SPI by two STM32 microcontrollers in my case, but you can program them directly using Sigma Studio)

Children
No Data