Post Go back to editing

A2B self-boot on EVAL-AD2428WD1BZ

Category: Software
Product Number: EVAL-AD2428WD1BZ
Software Version: A2B_Software-Rel19.3.1

Hi, 

I'm working with an hardware setup composed by an EVAL-AD2428WD1BZ, which is used as A2B master node, and some EVAL-AD2428WC1BZ boards (be A2B slaves).

And I construct my sigmaDSP on ADAU1452 & ADAU1761. It Works well so far.

 

Now, I want to set self-boot so that the hardware can automatically configure my A2B configuration and my sigmaDSPs when I start it somewhere else without my PC.

I refer to the documentations about self-boot, such as "EVAL-AD2428WD1BZ User Guide (Rev. 1.1).pdf"  and  "AE_09_A2B_SigmaStudio_UserGuide.pdf".

The following is what I do:

1. First, I uninstall the JP4 to make Self-Boot option enabled.

2. Assembled the hardware, open the A2B project to "Link Complie Download". Check everything is right.

3. Right click on the Target processor and selecting ‘Save Schematic in EEPROM’.

Then, click "Program". After waiting for a while, can see that it has been successfully stored in the EEPROM.

4. I think this should have completed the setting, so I unplug the power and replug.

 But nothig happened on my board. It doesn't even show signs of starting.

 

I must be doing something wrong.

Please someone can tell me in detail how to set self-boot.

Thanks



no
[edited by: p0800013 at 3:25 PM (GMT -4) on 2 Aug 2022]
Parents Reply Children