Post Go back to editing

There is a mismatch between the configured slave node and the actual connected node

Category: Software

I have a question I'd like to ask you:

Suppose that the A2B master node is configured through SigmaStudio and the three slave nodes are connected.

However, in practice, if only two slave nodes are connected and the a2B stack cannot work properly due to the discovery failure. Is this reasonable?

And, We hope that in this case, the actual connection of the two nodes can still work properly, such a requirement can be achieved?