Post Go back to editing

No audio from line out in EVAL-AD2428WD1BZ configured as slave

Hello,

I have a couple of questions regarding the setup I am working on.

First, I have an EVAL-AD2428WD1BZ set as master and another EVAL-AD2428WD!BZ configured as slave (I modified the jumper settings as mentioned in user guide). Using provided sample project file for 1761, I am enabling the test tone to output to line out (DAC0 and DAC1), but I am not hearing any audio output on speakers connected to line out of slave. The speaker when connected to the line out on master gives sound when test tone option is selected. This is just to test the line out.

Second, I have A2B slots set up on master and slave using stream config. I have digital audio sources in master ADAU 1452 output to different channels (say 500Hz to 0, 1, 2, 3). I am consuming these slots in the slave. How can I configure these inputs in Slave ADAU1761 to listen to different channels on line out of slave? How can I find out which inputs on 1761 map to A2B slots coming in?

Thank you for your time.

A

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.