Post Go back to editing

How is the TDM channel mapped to slots on the A2B bus?

Thread Summary

The user inquired about TDM channel mapping to A2B bus slots. The final answer provided a presentation for reference, detailing the mapping process. The user also asked if it's possible to consume and forward on the same slot on a slave node and if using a mask to select only odd slots would deliver the remaining even slots sequentially, noting the importance of the host driving channels for slave-1 before slave-0.
AI Generated Content
  • Please refer the attached presentation for understanding the TDM channel mapping to A2B bus slots.

  • Thanks for sharing a good materials, I am wondering if it's possible to both consume and forward on the same slot on a slave node.

    I'm also curious if, if I use a mask to select only the odd slots and consume them, the remaining even slots will be delivered sequentially. I'm asking this because of the statement in slice 3 of your materials that the host should make sure that channels for slave-1 are driven first and then channels for slave-0.

  • There are certain products that offer specific features that can be leveraged to generate the required output data.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.