简体中文 | 日本語
2 Replies Latest reply: Oct 17, 2011 11:27 AM by bootload RSS

ADuM5000 questions (CN-0159)

bootload Contributor
Currently Being Moderated

I am looking at Analog Devices Circuit Note CN-0159, the schematic on page 2 uses a ADuM5000

at location U2_C2. The schematic ties pin 11 ( no connect) to Viso and has the note. "DNP R10_C2

if U2_C2 is an AduM5000". The device in this location is a ADuM5000 and I see no reference to an

alternate device. My questions are 1, why is a no connect pin being tied high? I am gessing that there

is a alternate part that could be used. And the second question is what is DNP?

Thanks

 

Message was edited by: AndyR - Added Circuit Note number to title.

More Like This

  • Retrieving data ...

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 2 points