Add your comments about the Circuit Note found at http://www.analog.com/en/circuits-from-the-lab/CN0217/vc.html.
Questions or comments about CN0217, leave us your feedback here.
Hi, i've a problem with an evaluation circuit clone, sometimes there is like a glitch in the impedance curve. For example if i use a 560ohm as calibration resistance, with continuos sweep, sometimes the impedance trace shows a glitch only for one freq but not the same freq (e.s 200ohm @ 30kHz). Maybe a problem caused by the power supply, the layout or what?
thanks.
matteo
Hi Matteo,
Do you have a screen shot of this issue ? This is with the 16MHz crystal ?
Regards,
Liam
thanks,here the screen shot of the problem, the 16MHz maybe good enought, i've tried with two power supply for the 5V ( digital) and 12V for the analog but nothing.I've to check if there is a problem with analog and digital ground. thanks again.
-
Messaggio originale----
Da: analog@sgaur.hosted.jivesoftware.com
Data: 17-feb-2012 16.59
A: "Matteo Fattori"<matteo_fattori@virgilio.it>
Ogg: Re: CN0217: High Accuracy Impedance Measurements using 12-Bit Impedance Converters New message: "CN0217: High Accuracy Impedance Measurements using 12-Bit Impedance Converters" Re: CN0217: High Accuracy Impedance Measurements using 12-Bit Impedance Converters
EngineerZone
Re: CN0217: High Accuracy Impedance Measurements using 12-Bit Impedance Converters created by LiamR in Circuits from the Lab including SDP - View the full discussion
Hi Matteo,
Do you have a screen shot of this issue ? This is with the 16MHz crystal ?
Regards,
Liam
Reply to this message by replying to this email -or- go to the message on EngineerZone
Note: If you reply to this email, the entire email with the previous discussion and your signature will appear
in the posted reply, so you may want to remove this prior to sending the email.
Start a new discussion in Circuits from the Lab including SDP at EngineerZone
Hi,
Try breaking it into two excitation blocks, 1KHz to 20KHz and 20 KHz +.
For sub 5KHz we generally suggest reducing MCLK as per the User Guides recommendations.
Liam
How did you zoom in to the plot in figure 5?
Hi,
I used the download to excel tab and used the data on excel to generate a graph.Any luck with the external xtal oscillator that is on the board ?
liam
Hi, i've a question about the choice of Rfeedback (Rfb or sometimes called Rref): there is a way to use the right value of Rfb with a knowed Z to measure?I've see in one thesis that the suggestion is use the ratio Rfb/Zunk between 0,066-0,2. In others words Zunk must be 15/2 times the Rfb. I don't find this spec in the datasheet and specially the spec doesn't match with my test.
Now the question there is a way to calculate the error for a gived Zunk, and Rfb?With a gived Rfb wich is the measure span of Zunk ?
thanks
Hi imett,
Rfb sets the gain in the I-V amplifier.
Ideally, you should choose a Rfb value that generates less noise than the distortion of your impedance.
Remember, you are measuring harmonics so you don't want to hide harmonics due to the resistor noise.
Could you refer the thesis so I can read?
Regards,
Miguel
Sorry if I am repeating a known source. Macias' thesis is a nice and detailed application for AD5933 bioimpedance measurements:
http://bioimpedance.bme.ufl.edu/icebi/2760_Seoane.pdf
http://upcommons.upc.edu/pfc/bitstream/2099.1/7313/1/FDT_Raul_Macias_end_version.pdf
Regards,
Adnan Kurt