I recompiled and built the supplied shell_browser example for BF527, then I tried with 3 different USB Flash devices:
For the devices not working, the event ADI_USB_EVENT_RX_COMPLETE in HostEndpointZeroCompleteCallback( ) function doesn't happen.
Could someone give me some help on this problem?
Are there any additional modifications to the supplied example to have all the USB Flash devices working?
Is there any problem if size is greater than 256MB or filesystem not FAT?
I did other tests, and I have additional informations that I hope could help solving the problem:
/* IF (VBUS error Interrupt) */
if ( (ucIrqStatus&USB_INTRUSB_VBUSERROR_B) && pDev->Mode==MODE_OTG_HOST )
{
/* Acknowledge pending VBUS error interrupt */
*pUSB_INTRUSB = ucIrqStatus;
DriveVbusOff(pDev);
DriveVbusOn(pDev);
SetSessionBit();
return ADI_INT_RESULT_PROCESSED;
}
in UsbInterruptHandler() function (adi_usb_hdrc.c source file) are executed
This sounds me as an hardware problem....
Could someone give me some help?
Thanks
The Blackfin USB host mass storage software supports high speed USB memory sticks only, i.e. those that conform to the USB 2.0 spec. It may be that the sticks you are using are full speed (USB 1.1) devices.
Before we can investigate this further you need to provide us with as much detail (manufacturer, model number, etc) as possible for the failing USB sticks. Check also for the USB hi-speed logo on the packaging. In addition, please inform us of which VisualDSP++ 5.0 Update you are using.
Thanks
The following USB devices don't work
but they work perfectly on a PC (both Win and Linux).
I've been using VisualDSP++ 5.0 Update 6
I found in the silicon anomaly list some anomalies related to USB RX and BF527 rev 0.2. Could this be my problem?
Hi ,
I am also facing similar problem while using Transcend JetFlash v30 1GB.
Please find my observations,
1. adi_msd_usb_host_dev_def.CSCommand value is CS_GET_MAX_LUN
2. USB_EP_NI0_TXCSR valus is 804.
1 in bit position 2 indicates that control transaction is timeout.
So, I guess "Control transaction is time out during CS_GET_MAX_LUN command"
Is this observation correct?
Please suggest to solve the issue.
Thanks in advance,
D.Balabharathi
We have ordered some Transcend Drives and will investigate. We will let you know our results in due course.
regards
MartinK