简体中文 | 日本語
1 2 Previous Next 22 Replies Latest reply: Apr 22, 2012 9:54 PM by SimonB Go to original post RSS
  • 15. Re: compile linux for blackfin 548
    sonic Analog Employee
    Currently Being Moderated

    2008R1 is not supported, please use 2011R1 in native Linux env or Linux virtual machine instead.

  • 16. Re: compile linux for blackfin 548
    James.Kosin Regular Contributor
    Currently Being Moderated

    You can use coLinux, however, don't use a windows partition to untar or try to compile the sources on.  I've updated to a newer version of coLinux and had to modify to create a large coLinux partition to develop in... the sources are large.  But, even coLinux has problems with the windows partition and using linux tools on the partition.  You can get some very strange results and I haven't had any luck compiling linux on the windows partition without issues.

    The best bet is actually to install or use a full featured linux environment.

  • 17. Re: compile linux for blackfin 548
    AlexNikitin Contributor
    Currently Being Moderated

    I installing Ubuntu 11.10. Trying to compile linux, its compile 40 minutes and in the end I receive thats errors^

     

    CC  jffs2reader.o                                                     
    LD  jffs2reader                                                       
    CC  mkfs.ubifs/mkfs.ubifs.o                                         
    In file included from mkfs.ubifs/mkfs.ubifs.c:25:                         

    mkfs.ubifs/mkfs.ubifs.h:48:23: error: uuid/uuid.h: No such file or directory   

    mkfs.ubifs/mkfs.ubifs.c: In function 'write_data':                        

    mkfs.ubifs/mkfs.ubifs.c:1654: warning: implicit declaration of function 'time' 

    mkfs.ubifs/mkfs.ubifs.c: In function 'write_super':                       
    mkfs.ubifs/mkfs.ubifs.c:1967: warning: implicit declaration of function 'uuid_generate_random'                                                            
    mkfs.ubifs/mkfs.ubifs.c:1971: warning: implicit declaration of function 'uuid_unparse_upper'                                                              

    make[4]: *** [/mnt/cobd3/home/justice/blackfin-linux-dist/user/mtd-utils/build-36d8de81049c9c908740b690c664b5bd3703ccd6-host/mkfs.ubifs/mkfs.ubifs.o] Error 1  

    make[4]: Leaving directory `/mnt/cobd3/home/justice/blackfin-linux-dist/user/mtd-utils/36d8de81049c9c908740b690c664b5bd3703ccd6'                          
    make[3]: *** [all] Error 2                                                
    make[3]: Leaving directory `/mnt/cobd3/home/justice/blackfin-linux-dist/user/mtd-utils'                                                                   
    make[2]: *** [mtd-utils] Error 2                                          

    make[2]: Leaving directory `/mnt/cobd3/home/justice/blackfin-linux-dist/user'  

    make[1]: *** [all] Error 2                                                

    make[1]: Leaving directory `/mnt/cobd3/home/justice/blackfin-linux-dist/user'   make: ***

    [subdirs] Error 1                                               

    colinux:/mnt/cobd3/home/justice/blackfin-linux-dist#  

  • 18. Re: compile linux for blackfin 548
    Aaronwu Analog Employee
    Currently Being Moderated

    What your uClinux distribution version please, we recommend the 2011R1, old versions are usually not supported, and make sure you have proper packages installed on your Ubuntu host as described in http://docs.blackfin.uclinux.org/doku.php?id=installing_linux

  • 19. Re: compile linux for blackfin 548
    AlexNikitin Contributor
    Currently Being Moderated

    Yes. Toolchain and uLinux downloaded from blackfin.uclinux.org. All 2011 versions

  • 20. Re: compile linux for blackfin 548
    Aaronwu Analog Employee
    Currently Being Moderated

    try this: apt-get install uuid-dev

  • 21. Re: compile linux for blackfin 548
    AlexNikitin Contributor
    Currently Being Moderated

    It seems help. You must add this to instruction! Thanks!

  • 22. Re: compile linux for blackfin 548
    SimonB Analog Employee
    Currently Being Moderated
1 2 Previous Next

More Like This

  • Retrieving data ...

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 2 points