简体中文 | 日本語
3 Replies Latest reply: Apr 4, 2012 11:39 AM by Reemo RSS

AD8264 crosstalk spec?

dlewis Member
Currently Being Moderated

What is the crosstalk specification? or is there any test data on crosstalk between the analog channels on the AD8264?

 

Thanks in advance

 

Dave

  • 1. Re: AD8264 crosstalk spec?
    harryh Analog Employee
    Currently Being Moderated

    dlewis,

     

      There is a figure 52 on the AD8622/8624 datasheet that shows the crosstalk on the dual.

    For any part from any manufacturer, it is important to know how it was tested.  If you consider

    one of the sections to be the transmitter, and another section to be the receiver, then you want

    a heavy load on the transmitter, and no load on the receiver.  With what we have learned about

    layout in the past 30-40 years, the duals and quads today are pretty good.  Because of this,

    the interference from the transmitter is very small, so you want to take gain in the receiver.

    Note that figure 52 uses a 10k load on the transmitter.  The AD8622/8624 is a low power part,

    so the spec tables have Voh and Vol specified with 10k and 100k loads.  Thus, fig 52 uses

    a 10 load.  The gain on the receiver is +101.  When we graph the data, we take this into account,

    so the dB scale is input refered.

     

    The low frequency crosstalk is a thermal effect, the power dissipation in the output stage of the

    transmitter travels across the die and unbalances the input stage on the receiver.  The high frequency

    cross talk is generally a capacitive effect, both in the test setup, but also the capacitance to substrate

    for all the transistors in a junction-isolated part.

     

    Another disadvange of using quads, especially with active filters, is you wind up with 20 passives

    crowded around a tiny package, and the pc board trace to trace capacitance is a killer.

     

    If you need extremely good numbers, then using duals or even singles would be the way to go.

    See the article(s) below for more details.

     

    Harry

     

    http://www.eetimes.com/design/analog-design/4210663/Op-amps--to-dual-or-not-to-dual---Part-1-of-2-

     

    http://www.eetimes.com/design/analog-design/4210881/Op-amps--to-dual-or-not-to-dual---Part-2-of-2-

  • 2. Re: AD8264 crosstalk spec?
    dlewis Member
    Currently Being Moderated

    Hi Harry

     

    Thanks but I was asking about the AD8264 quad differential VGA Amplifier not the AD8624?

     

    Thanks

     

    Dave

  • 3. Re: AD8264 crosstalk spec?
    Reemo Analog Employee
    Currently Being Moderated

    Hi Dave,

     

    Unfortunately, we don't have any test data for crosstalk on the AD8264. Of course, we would design it to minimize crosstalk as much as possible, but we have no data to quantify that for you. If you run into any issues, please do let us know and we'll work with you on it..

     

    Reemo

More Like This

  • Retrieving data ...

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 2 points