EngineerZone
All Places
Processors and DSP
Software and Development Tools
Linux Distribution for Blackfin
Discussions
Hello,
I have the following hardware setup:
cm-bf561, evaluation kit and camera extender board from bluetechnix. camera: ov7670 and ov2640
Software setup:
uclinux distribution: 2011R1-RC3.
menuconfig set up as per http://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:v4l2_blackfin_capture
Did settings as per the above link for ov2640
Problem:
No video0 device is created after modprobe bfin-video-capture
How should I get the v4l2 to work and grab an image?
Also I tried to port v4l1 from 2010 distribution, but that gives a memory exception while trying to grab an image.
Is the v4l previous framework compatible with the new kernel?
ovXXXX sensors are not enabled and tested in Blackfin Linux kernel. If you want to use them, you should add proper ovXXXX bfin_capture platform data into your cm-bf561 board file by your self.
Thank you for your answer.
Could you please help me as to how I can do that or if there is an example that I can follow?
Also do you know if V4L1 will be compatible on the new kernel? I have replaced the complete video folder in the drivers/media under the linux kernel tree and compiled the code but when I try to grab an image, it gives me memory errors such as the following:
Stack info:
SP: [0x020abf24] IM `;1
Memory from 0x020abf20 to 020ac000
020abf20: 025fff70 [0254ceb0] 00008000 00000000 00000000 020ac000 0254ceb0 0254ceb0
020abf40: 02082840 001098ec 02003004 0255da6d 0258c5bf 0255da22 0258c5be 00000000
020abf60: 00000000 00000083 00000000 00000083 00000000 00000000 7ffff000 000000c0
020abf80: 00000137 00000000 00000000 00000000 00000000 0000005b 00001802 00000001
020abfa0: fffffffc 00000006 00000003 02082990 02082918 025ffc9c 025ffca8 0253d188
020abfc0: 025b75b8 0253d188 025b7294 0254cea4 00000036 025fff9d 025fff50 025fff70
020abfe0: 00000001 0000cea4 025ffcd8 803c7601 00000003 00000003 00000036 00000006
Return addresses in stack:
Modules linked in: blackfin_cam videodev v4l1_compat ov7673
Kernel panic - not syncing: Kernel exception
Stack info:
SP: [0x020abcf4]
Please refer to linux-kernel/arch/blackfin/mach-bf561/board/ezkit.c
Search BLACKFIN_CAPTURE.
You should match platform data with your hardware design.
V4L1 has been removed from the new kernel. You can refer to drivers/media/video/vs6624.c as an example sensor driver.
Thank you everyone for your answers.
I have tried to understand the ezkit.c but the parameters related to adv7183 that are present, I am not sure I understand what they are for.
static struct v4l2_input adv7183_inputs[] = {
static struct bcap_route adv7183_routes[] = {
what are these structures used for?
Is there a similar configuration for ovXX series present somewhere that I can go through?
I also tried to follow the vsXX series but that is not supported in the ezkit.c so I am guessing, it will anyway not work
ezkit.c is a board file where you pass some board specific parameters to the driver. adv7183.c is the real driver but it is a decoder driver. vs6624.c is a sensor driver which is similar to ov sensors.
adv7183_input is the input array adv7183 can support. adv7183_routes is the route of each input.
Thank you for your reply.
So do I need to add anything related to the sensor in the ezkit.c.
If yes, then what is it that I need to add, in order to make it work
Considering you are talking about ov sensors, I have to say I can't tell you details. What you need to do is to write an ov sensor driver and pass in parameters that are requested in your driver. Please refer to Documentation/video4linux/v4l2-framework.txt as a start.