This Question is Not Answered

1 "correct" answer available (4 pts) 2 "helpful" answers available (2 pts)
3 Replies Last post: Jul 2, 2009 1:38 AM by sunil inaganti  
sunil inaganti Contributor 16 posts since
Jun 16, 2009
Currently Being Moderated

Jul 1, 2009 9:03 AM

Audio Extender with BF-533 EZ-Kit Lite

Hi,

         We are using Audio extender card with BF-533 Ez-Kit Lite. We are receving digital data through ADAV801 and SPOrt0.

This data is transmitting through AD1938 on Sport1.

 

        We have provided 0-db sine tone as input, Then in the output we have observed -12db difference in amplitue level. When we check in Sport1Tx  buffer, we found 0x7FFF000, means no attenuation in the receiver. So, problem can be in ADAV1938.

 

         Anybody is having idea whether AD1938 will provide any attenuation.

 

with regards,

sunil

TomA Analog Employee   20 posts since
Mar 17, 2009
Currently Being Moderated
1. Jul 1, 2009 11:24 AM in response to: sunil inaganti
Re: Audio Extender with BF-533 EZ-Kit Lite

Hello Sunil,

 

Some possible reasons why you may be seeing this:

 

  1. Looking at the typical performance characteristics (in the datasheets) of both devices, for the DAC and ADC components respectively, there is a varied response depending on what frequency you are trying to pass. I'd bet that if you varied the frequency of the sine wave, you would see varying attenuation levels, based on comparing these basic frequency response plots.
  2. The analog conditioning circuitry on the Audio Ez-extender, both for the DAC output and the ADC input (op-amp and discretes) will definitely have an effect on frequency response. I can't say what the effect is without modeling the circuit, but if modeled, it would be possible to obtain some idea of how this circuitry affects the attenuation of the DAC output and scales the signal to the ADC input.

 

If you would like more specific information on the converters (AD1938 and ADAV801) I'd recommend you contact Linear Applications Support through their email support system:

https://form.analog.com/Form_Pages/support/standard_linear/contacttechSupport.aspx

 

Hope this helps.

 

Regards,

Tom

gyi Analog Employee   36 posts since
Mar 12, 2009
Currently Being Moderated
2. Jul 1, 2009 11:49 AM in response to: sunil inaganti
Re: Audio Extender with BF-533 EZ-Kit Lite

Hi Sunil,

 

Are registers 6-13 (DAC volume control) on the 1938 set to 0 for no attenuation?

 

Regards,

 

Gabby

More Like This

  • Retrieving data ...