This Question is Possibly Answered

1 "correct" answer available (4 pts) 1 "helpful" answer available (2 pts)
20 Replies Last post: Sep 9, 2009 10:01 AM by boris liberol   1 2 Previous Next
Christoph Pfeiffer Contributor 44 posts since
Jun 5, 2009
Currently Being Moderated

Jun 23, 2009 9:47 AM

very fast CRC32 code wanted

is there any highly optimized crc32 algorithm for BF537?

i need a very fast implementation

regards chris

Thomas Ireland Contributor 6 posts since
Jun 23, 2009
Currently Being Moderated
1. Jun 23, 2009 2:22 PM in response to: Christoph Pfeiffer
Re: very fast CRC32 code wanted

Would crc16 be good enough? If you put the internal vars as registers and if it is small enough, make sure the target data is in cashe it should be really quick.

ystein Analog Employee   8 posts since
Aug 19, 2009
Currently Being Moderated
3. Sep 1, 2009 10:40 AM in response to: Christoph Pfeiffer
Re: very fast CRC32 code wanted

Chris,

As a starting point you can use Yaniv’s “Efficient CRC calculation with minimal memory footprint”

, Embedded.com, 03/16/2008 article that shows how to implement any CRC up to 32bit (included) in two cycles per bit.

http://www.embedded.com/design/206901030?printable=true

Thanks,

Ystein

BennoK Analog Employee   6 posts since
Jun 9, 2009
Currently Being Moderated
4. Sep 1, 2009 12:40 PM in response to: ystein
Re: very fast CRC32 code wanted

or check the sources of the BF54x boot code which come with your VisualDSP++ installation

Paul Beckmann Contributor 6 posts since
May 29, 2009
Currently Being Moderated
5. Sep 1, 2009 5:39 PM in response to: BennoK
Re: very fast CRC32 code wanted

We use a basic CRC check on the Blackfin.  To send a N word array, we add on a single 32-bit so that when everything is xor'ed together, you end up with zero.  This is good for catching any single word error.  It's fast as well.  The code snippet is:

 

{

     DWORD crc=0;

     for(i=0; i<nLen; i++)

          {

          crc^=g_PacketBuffer[i];

          }

     if (crc != 0)

          goto Packet_Error;

}

ystein Analog Employee   8 posts since
Aug 19, 2009
Currently Being Moderated
6. Sep 1, 2009 8:22 PM in response to: Paul Beckmann
Re: very fast CRC32 code wanted

Paul,

 

The algorithm that you are presenting called longitudinal parity check, which breaks the data into "words" with a fixed number n of bits, and then computes the XOR of all those words. The result is appended to the message as an extra word. To check the integrity of a message, the receiver computes the exclusive or of all its words, including the checksum; if the result is not a word with n zeros, the receiver knows that a transmission error occurred.

With this checksum, any transmission error that flips a single bit of the message, or an odd number of bits, will be detected as an incorrect checksum. However, an error that affects two bits will not be detected if those bits lie at the same position in two distinct words.

 

On the other hand:

 

CRC is along division operation in which the quotient is discarded and the reminder becomes the result, with the important distinction that the arithmetic used is the carry-less arithmetic of a finite field GF(2). Typically, an n-bit CRC, applied to a data block of arbitrary length, will detect any single error burst not longer than n bits (in other words, any single alteration that spans no more than n bits of the data).

Thanks,

Yosi

Sean M Analog Employee   24 posts since
Apr 17, 2009
Currently Being Moderated
7. Sep 2, 2009 6:11 AM in response to: Christoph Pfeiffer
Re: very fast CRC32 code wanted

Just ran into something in the Blackfin Programming Reference, remembered this thread and decided it might be worth bringing it up. There's a couple of instructions, BXOR and BXORSHIFT, which have a Type I CRC as an example of their usage. You would need to make a couple of adjustments (CRC_LEN would have to be 32, and you'd have to alter the code to be callable from C - receiving a ptr to the message as a parameter etc), however it might at the very least give you ideas. I've copied the text from the PRM below:

The BXOR and BXORSHIFT instructions let you calculate a Type I
CRC at a rate of two cycles per input bit, as in the following example
program:

 

// _CRC_BXOR - calculate CRC value of a message polynomial
// for a given generator polynomial.
#define MSG_LEN 32 // bits
#define CRC_LEN 16 // bits


_CRC_BXOR:
a1 = a0 = 0;
r1 = 0x8408 (z); // LFSR polynomial, reversed:

                 // x^16 + x^12 + x^5 + 1


a1.w = r1; // initialize LFSR mask
r2.h = 0xd065; // r2 = message
r2.l = 0x86c9;
p1 = MSG_LEN (z);


loop _MSG_loop lc0 = p1;
loop_begin _MSG_loop;
r2 = rot r2 by 1;
a0 = bxorshift(a0, a1, cc);
loop_end _MSG_loop;


r0 = 0; // initialize CRC
r2.l = cc = bxor(a0, r1);
r0 = rot r0 by 1;
p1 = CRC_LEN-1 (z);


loop _CRC_loop lc0 = p1;
loop_begin _CRC_loop;
r2.l = cc = bxorshift(a0, r1);
r0 = rot r0 by 1;
loop_end _CRC_loop;
// r0.l now contains the CRC
_CRC_BXOR.end:

Hazarathaiah Malepati Analog Employee   4 posts since
Jul 16, 2009
Currently Being Moderated
8. Sep 2, 2009 2:11 PM in response to: Sean M
Re: very fast CRC32 code wanted

Hi,

 

Using 1 kB data memory, we can implement CRC32 on Blackfin with 1 cyc/bit.

 

-mahana

Yaniv Sapir Analog Employee   14 posts since
Aug 14, 2009
Currently Being Moderated
9. Sep 2, 2009 3:58 PM in response to: Sean M
Re: very fast CRC32 code wanted

The code above, from Sean's post, is similar to the article Yosi pointed to earlier. In the article one can find detailed explanation on how to adjust this kind of code to specific needs.

Yaniv Sapir Analog Employee   14 posts since
Aug 14, 2009
Currently Being Moderated
10. Sep 2, 2009 3:57 PM in response to: Hazarathaiah Malepati
Re: very fast CRC32 code wanted

Mahana,

 

I guess it would be nice to post a code sample.

Sean M Analog Employee   24 posts since
Apr 17, 2009
Currently Being Moderated
11. Sep 2, 2009 5:03 PM in response to: Yaniv Sapir
Re: very fast CRC32 code wanted

Heh, I should really have looked at the embedded.com article you posted as it's pretty much the same as the PRM text.

Yaniv Sapir Analog Employee   14 posts since
Aug 14, 2009
Currently Being Moderated
12. Sep 2, 2009 8:09 PM in response to: Sean M
Re: very fast CRC32 code wanted

LOL! I wonder why...

boris liberol Analog Employee   13 posts since
Aug 19, 2009
Currently Being Moderated
13. Sep 3, 2009 11:36 AM in response to: Yaniv Sapir
Re: very fast CRC32 code wanted

Hi Yaniv,

 

 

WIth LUT, it could work like this -

 


/* algorithm:

   new CRC (updated each incoming byte) = (old CRC << 8) ^ (CRC_update_table[input byte ^ MSByte of old CRC] )

*/

// ... proper loading the loop, then:

 

// CRC lives in R0

 

CRC32Start:
  
   r3 = r2 << 2      || r6 = [p1];    // r6 is 32-bit CRC corresponding to input byte^MSbyte of CRC
   r3 = r7 + r3 (ns) || r1 = b[p0++]; // r7 - base  for CRC update table, r1 - input byte
   p1 = r3;                           // ptr into CRC update table, size 256*4 bytes
  
   r5 = r0 >> 24;  // 8 MSB of CRC interacting with input
   r2 = r1 ^ r5;
  
   r5 = r0 << 8;  // 24 LSB of old CRC interacting with CRC update         
CRC32End:  
   r0 = r5 ^ r6;   
  
   // 7 cycles per 8 bits = 0.875 c/bit

 

boris.liberol@analog.com

ystein Analog Employee   8 posts since
Aug 19, 2009
Currently Being Moderated
14. Sep 3, 2009 3:09 PM in response to: boris liberol
Re: very fast CRC32 code wanted

Boris,

Do you agree that the two LSB of R7 are "0" (32bit aligned!)

You can save a cycle by:

 

Mine  R7 == yours >>2!!!

 

 

// CRC lives in R0

CRC32Start:

 

  r3 = (r7+r2) << 2      || r6 =[p1];           // r7 = CRC table base , r6 is 32-bit CRC corresponding to input byte^MSbyte of CRC

  p1 = r3;                                            // ptr into CRC update table, size 256*4 bytes

 

  r5 = r0 >> 24 ||  r1 = b[p0++];            // r1 - input byte,  8 MSB of CRC interacting with input

  r2 = r1 ^ r5;

 

  r5 = r0 << 8;                                    // 24 LSB of old CRC interacting with CRC update

CRC32End:

  r0 = r5 ^ r6;

 

and now you have 6 cyc/8bit == > 0.75cyc/bit

 

do you agree?

 

Thanks,

Yosi

 

 

More Like This

  • Retrieving data ...