This FAQ applies to EVAL-ADV7619-7511 and EVAL-ADV7619-7511P. All support files in their latest versions will be attached below.
Below are the support files for these evaluation boards. If you use these files, we recommend that you subscribe to EMail notifications for either the entire forum or at least this FAQ by clicking on the menu to the right. In this way you will be automatically notified if there are any comments or changes to this FAQ or attached documents. If the menu choice is "Stop email notifications," then you are already subscribed.
| File | Content |
|---|---|
| EVAL-ADV7619-7511_rev1p1.pdf | Schematics (PDF) for EVAL-ADV7619-7511/EVAL-ADV7619-7511P |
| EVAL-ADV7619-7511_build_files.zip | This zip contains ORCAD schematic, Allegro board files, gerbers, and BOMs for the evaluation boards |
| UG-nnn_Rev0_prelim.pdf | Preliminary User Guide for the EVAL-ADV7619-7511 |
| EVAL-ADV7619-7511_v1p1_firmware.zip | Zip file with current firmware images. The *.bin file is the application which can be flashed with UBOOT with normal RS-232 and a terminal program. The hex file contains the applicaition and UBOOT and to load this on the board you will need at least ADZS-ICE-100B and the test drive version of VisualDSP++ |
| AVES | Evaluation software for the board |
| AdvantivVideo.zip | USB Driver for Advantiv™ Video Evaluation Boards |
Comments