简体中文 | 日本語
Currently Being Moderated

Advantiv™ EVAL-ADV7612-7511 Video Evaluation Board

This FAQ applies to EVAL-ADV7612-7511 and EVAL-ADV7612-7511P. All support  files in their latest versions will be attached below.

 

Below are the support files for these evaluation boards. If you use these files, we recommend that you subscribe to EMail notifications for  either the entire forum or at least this FAQ by clicking on the menu to the  right.  In this way you will be automatically notified if there are any  comments or changes to this FAQ or attached documents.  If the menu choice is  "Stop email notifications," then you are already subscribed.

 

 

FileContent
EVAL-ADV7612-7511_rev0p1_schems.pdfSchematics (PDF) for EVAL-ADV7612-7511/EVAL-ADV7612-7511P
EVAL-ADV7612-7511_build_files.zipThis zip contains ORCAD schematic, Allegro board files, gerbers, and BOMs for the evaluation boards
UG-295User Guide for the EVAL-ADV7612-7511
EVAL-ADV7612-7511_v1p2_boot_image.zipComplete firmware image for EVAL-ADV7612-7511 including u-boot bootloader and v1p2 application binary. In order  to program this on the board you will need at least ADZS-ICE-100B and the test drive version of VisualDSP++. This file is in Intel-Hex format.
EVAL-ADV7612-7511P_v1p2_boot_image.zip

Complete firmware image for EVAL-ADV7612-7511P including u-boot bootloader and v1p2 application binary. In order  to program this on the board you will need at least ADZS-ICE-100B and the test drive version of VisualDSP++. This file is in Intel-Hex format.

EVAL-ADV7612-7511_v1p2_app.zipApplication binary v1p2 for EVAL-ADV7612-7511. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide UG-295.
Note: This file is in binary format in order to be compatible with u-boot.
EVAL-ADV7612-7511P_v1p2_app.zipApplication binary v1p2 for EVAL-ADV7612-7511P. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide UG-295.
Note: This file is in binary format in order to be compatible with u-boot.
AVESEvaluation software for the board
AdvantivVideo.zipUSB Driver for Advantiv™ Video Evaluation Boards

Comments

Delete FAQ

Are you sure you want to delete this FAQ?