简体中文 | 日本語
Currently Being Moderated

Advantiv™ EVAL-ADV7842-7511 Video Evaluation Board

This FAQ applies to EVAL-ADV7842-7511 and EVAL-ADV7842-7511P. All support files in their latest versions will be attached below.

 

Below are the support files for these evaluation board. We recommend that, if you download and use these files, you subscribe to EMail notifications for either the entire forum or at least this FAQ by clicking on the menu to the right.  In this way, you will be automatically notified if there are any comments or changes to this FAQ or attached documents.  If the menu choice is "Stop email notifications," then you are already subscribed.

 

 

FileContent
EVAL-ADV7842-7511_Rev1p0.pdfThis is the current version of the schematics for the eval board.  The PCB may say REV 1.1, this is the correct schematic for that PCB.
EVAL-ADV7842-7511_build_files.zipThis zip contains ORCAD schematic, Allegro board files, gerbers, and BOMs for the evaluation boards
UG-235User guide for the EVAL-ADV7842-7511
EVAL-ADV7842-7511_v1p1_boot_image.zip

Complete firmware image for EVAL-ADV7842-7511 including u-boot bootloader and v1p1 application binary. In order to program this on the board you will need at least ADZS-ICE-100B and the test drive version of VisualDSP++. This file is in Intel-Hex format.

EVAL-ADV7842-7511_v1p54_boot_image.zip

Complete firmware image for EVAL-ADV7842-7511 including u-boot bootloader and v1p54 application binary. In order to program this on the board you will need at least ADZS-ICE-100B and the test drive version of VisualDSP++. This file is in Intel-Hex format.

EVAL-ADV7842-7511P_v1p1_boot_image.zip

Complete firmware image for EVAL-ADV7842-7511P including u-boot bootloader and v1p1 application binary. In order to program this on the board you will need at least ADZS-ICE-100B and the test drive version of VisualDSP++. This file is in Intel-Hex format.

EVAL-ADV7842-7511_v1p1_app.zip

Application binary v1p1 for EVAL-ADV7842-7511. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide UG-295. This file is in binary format.

EVAL-ADV7842-7511_v1p54_app.zipApplication binary v1p1 for EVAL-ADV7842-7511. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide UG-295. This file is in binary format.
EVAL-ADV7842-7511P_v1p1_app.zipApplication binary v1p1 for EVAL-ADV7842-7511P. If your board has a functional u-boot bootloader, you can program this on the board via RS232 following the instructions in the user guide UG-295. This file is in binary format.
AVES

This is the installer for the Evaluation software mentioned in the User guide.

Hardware Config Update for Rev 1p0_1p1.pdf

Hardware Configuration Update for using component video with Revision 1.1 versions of the eval board.

(Note: If YPbPr / Component Video is important for your application, read this first!)

AdvantivVideo.zipUSB Driver for Advantiv™ Video Evaluation Boards

Comments

Delete FAQ

Are you sure you want to delete this FAQ?